SLUUD99A February 2025 – April 2025 BQ25858-Q1 , BQ25858B-Q1
The following list of equipment is recommended when testing with a constant voltage electronic load.
A power supply capable of supplying 40V at 8A is required. While this part can handle larger voltage and current, larger power levels are not necessary for this procedure.
An Eload: Kikusui PLZ164WA 0-150V, 0-33A, or equivalent
Six Fluke 75 multimeters, (equivalent or better) or: Three equivalent voltage meters and three equivalent current meters.
A computer with at least one USB port and a USB cable.
For software setup, refer to section 2.4.