SLVAF85 September 2026 TPS2596 , TPS25961
As shown in Figure 3-1, the proposed design replaces the RLIM resistor with an eFuse. Unlike the conventional RC-based design where the supply current is limited by RLIM, the eFuse allows the current limit to be programmed through the ILIM pin. A higher current limit enables the power supply to deliver more energy during latching, thereby reducing the required hold-up capacitance.
The required hold-up capacitance can be calculated using Equation 2:
In a typical single phase smart e-meter:
A 1.5mF hold-up capacitor is required for successful latching under the above typical operating conditions, as calculated using Equation 2.
The minimum hold-up capacitance required at various eFuse current-limit settings was calculated, and the corresponding test results are shown in Figure 3-2 to Figure 3-4.
The test results in Figure 3-2 to Figure 3-4 show that increasing the current limit reduces the required hold-up capacitance. Therefore, the capacitor size is primarily determined by the current limit during the latching phase.
A dynamic current limit method can further optimize both capacitor size and power consumption by configuring a higher current limit during latching and a lower limit during steady-state operation. This allows the SMPS to provide maximum available energy during latching while reducing the steady current during steady state. The dynamic current implementation is described below and shown in Figure 3-5.
Implementation of dynamic current limit:
The dynamic current-limiting tests were performed with the lower current limit fixed at 120mA and different higher current-limit values. A 5V DC gate signal was applied to the N-channel MOSFET for 50ms to enable the higher current limit. After 50ms, the current limit returned to 120mA in each test. The corresponding test results are shown in Figure 3-6 and Figure 3-7.
Consider the implementation circuit corresponding to the test results shown in Figure 3-7. The inrush current limit is set to 120mA, while the latching-phase current limit is set to 180mA. With dynamic current limiting, the required hold-up capacitor is 0.69mF, compared with 3.3mF used in the conventional non-eFuse design.