SLVAFE6 December 2022 TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPS6287B10 , TPS6287B25 , TPSM8287A06 , TPSM8287A12 , TPSM8287A15
At converters having a fixed output voltage, the output voltage usually cannot be configured in a simple way. Devices of the TPS6287x family support selecting a predefined output voltage using an appropriate configuration at the VSEL pin. If the desired output voltage cannot be selected using VSEL, the output voltage still can be programmed using the digital interface once the device is powered properly. This change can be done before the device is enabled. After enable, the device starts into the newly programmed output voltage. Additional details can be found in the TPS6287x-Q1 2.7-V to 6-V Input, 6-A, 9-A, 12-A, 15-A, Automotive, Stackable, Synchronous Step-Down Converters with Fast Transient Response data sheet.
If this process cannot be done, for example, if there is no interface communication possible since the host for the interface is not active before or during startup, other means of addressing that are required. This application note explains how this problem can be addressed using a resistor divider. This application note also explains the limitations of this approach.