SLVAFV8A July 2024 – July 2025 TPS25751
The image file generated from the GUI was slightly modified as shown in the following code.
#include "ti_msp_dl_config.h"
#include "lrb.h"
const uint8_t tps25751_lowRegion_i2c_array[SIZEOFLRB] = {
0x01, 0x00, 0xe0, 0xac, 0xfe, 0xff, 0xff, 0xff, 0x80, 0x06, 0x00, 0x00, 0x00, 0x26, 0x00, 0x00,
0x71, 0x3e, 0x9c, 0xb8, 0x00, 0x00, 0x00, 0x00, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
...
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
The file, lrb.h, is shown in the following code for context.
#define SIZEOFLRB 0x2C80 // 11392
/* Maximum size of TX packet, MCU 0xFFF */
#define I2C_TX_MAX_PACKET_SIZE
/* SIZEOFLRB/I2C_TX_MAX_PACKET_SIZE +1 */
#define LRB_NUMBER_OF_PACKETS (0x0003)
/* SIZEOFLRB % I2C_TX_MAX_PACKET_SIZE */
#define LRB_REMAINDER (0x0C82)
extern const uint8_t tps25751_lowRegion_i2c_array[SIZEOFLRB];
The following example code is based upon the MSPM0C110x Driver Library(1) and the steps found in Section 4.1.
/*
* 1. Wait for Ready for Patch interrupt
*/
debounce = 1;
/* Skip glitch at boot */
while(debounce)
{
while(DL_GPIO_readPins(
GPIO_SWITCHES_PORT, GPIO_SWITCHES_USER_SWITCH_1_PIN));
delay_cycles(DELAY_500us);
if(!DL_GPIO_readPins(
GPIO_SWITCHES_PORT, GPIO_SWITCHES_USER_SWITCH_1_PIN))
{
debounce = 0;
}
}
/*
* 2. Mode == PTCH
*/
readRegister(MODE_REGISTER, MODE_BYTE_CNT, gRxPacket);
if(gRxPacket[1] != 0x50)
{
delay_cycles(DELAY_10ms);
readRegister(MODE_REGISTER, MODE_BYTE_CNT, gRxPacket);
}
/*
* 3a. Configure I2Ct_IRQ for CMD1 Complete
*/ */
gTxPacket = (uint8_t*)maskIntReg;
writeRegister(INT_BYTE_CNT, (uint8_t*)gTxPacket);
waitingForPD = 1;
while(waitingForPD)
{
/*
* 3b. Clear Interrupts
*/
gTxPacket = (uint8_t*)clrIntReg;
writeRegister(INT_BYTE_CNT, (uint8_t*)gTxPacket);
// Wait for interrupt to clear
while(DL_GPIO_readPins(GPIO_SWITCHES_PORT, GPIO_SWITCHES_USER_SWITCH_1_PIN)==0);
waitingForGoodData = 1;
while(waitingForGoodData)
{
/*
* 4. Send PBMs Data
*/
gTxPacket = (uint8_t*)PBMsData;
writeRegister(DATA_BYTE_CNT, gTxPacket);
delay_cycles(DELAY_500us);
/*
* 5. Data Good
*/
readRegister(DATA_REG, (DATA_BYTE_CNT-1), gRxPacket);
if(gRxPacket[1] == 0x80)
{
waitingForGoodData = 0;
}
}
/*
* 6. Send PBMs to CMD1
*/
gTxPacket = (uint8_t*)PBMsCmd;
writeRegister(CMD_BYTE_CNT, gTxPacket);
/*
* 7. Wait for I2Ct_IRQ
*/
while(DL_GPIO_readPins(
GPIO_SWITCHES_PORT, GPIO_SWITCHES_USER_SWITCH_1_PIN));
/*
* 8. CMD1 Clear
*/
readRegister(CMD_REG, (CMD_BYTE_CNT-1), gRxPacket);
/*
* 9. DATA1 Clear
*/
readRegister(DATA_REG, (DATA_BYTE_CNT-1), gRxPacket);
if(gRxPacket[1] == 0x0)
{
waitingForPD = 0;
}
}
/*
* 10. Burst Data
*/
ii = LRB_NUMBER_OF_PACKETS;
while(ii)
{
if(ii == 1)
{
gTxLen = LRB_REMAINDER;
}
else
{
gTxLen = I2C_TX_MAX_PACKET_SIZE;
}
/* The FIFO is 8-bytes deep, and this function returns number of bytes written to FIFO */
gTxPacket = (uint8_t*)&tps25751_lowRegion_i2c_array[(LRB_NUMBER_OF_PACKETS-ii)*I2C_TX_MAX_PACKET_SIZE];
ii = ii-1;
gTxCount = DL_I2C_fillControllerTXFIFO(I2C_INST, gTxPacket, gTxLen);
DL_I2C_enableInterrupt(
I2C_INST, DL_I2C_INTERRUPT_CONTROLLER_TXFIFO_TRIGGER);
gI2cControllerStatus = I2C_STATUS_TX_STARTED;
while (!(
DL_I2C_getControllerStatus(I2C_INST) & DL_I2C_CONTROLLER_STATUS_IDLE))
;
DL_I2C_startControllerTransfer(
I2C_INST, I2C_TGT_BURST_ADDRESS, DL_I2C_CONTROLLER_DIRECTION_TX, gTxLen);
while ((gI2cControllerStatus != I2C_STATUS_TX_COMPLETE) &&
(gI2cControllerStatus != I2C_STATUS_ERROR)) {
__WFE();
}
while (DL_I2C_getControllerStatus(I2C_INST) &
DL_I2C_CONTROLLER_STATUS_BUSY_BUS)
;
/* Trap if there was an error */
if (DL_I2C_getControllerStatus(I2C_INST) &
DL_I2C_CONTROLLER_STATUS_ERROR) {
__BKPT(0);
}
while(!(
DL_I2C_getControllerStatus(I2C_INST) & DL_I2C_CONTROLLER_STATUS_IDLE))
;
delay_cycles(DELAY_500us);
}
/*
* 11. Clear Interrupts
*/
gTxPacket = (uint8_t*)clrIntReg;
writeRegister(INT_BYTE_CNT, (uint8_t*)gTxPacket);
// Wait for interrupt to clear
while(DL_GPIO_readPins(
GPIO_SWITCHES_PORT, GPIO_SWITCHES_USER_SWITCH_1_PIN)==0)
;
/*
* 12. Send PBMc to CMD1 Register
*/
gTxPacket = (uint8_t*)PBMcCmd;
writeRegister(CMD_BYTE_CNT,gTxPacket);
/*
* 13. I2Ct_IRQ == Low, CMD1 complete
*/
while(DL_GPIO_readPins(
GPIO_SWITCHES_PORT, GPIO_SWITCHES_USER_SWITCH_1_PIN));
/*
* 14. Read CMD1
*/
readRegister(CMD_REG, (CMD_BYTE_CNT-1), gRxPacket);
/*
* 15. Delay 20ms
*/
delay_cycles(DELAY_20ms);
/*
* 16. Read Data1
*/
readRegister(DATA_REG, 0x28, gRxPacket);
/*
* 17. MODE === APP
*/
waitingForPD = 1;
while(waitingForPD)
{
readRegister(MODE_REGISTER, MODE_BYTE_CNT, gRxPacket);
if(gRxPacket[1] == 0x41)
{
waitingForPD = 0;
}
else
{
delay_cycles(DELAY_10ms);
}
}