SLVAG00 January 2026 BZX84C15V
In this example we select a zener diode to prevent an enhancement mode N-channel MOSFET's gate-to-source maximum voltage rating from being exceeded. The input voltage is 12V with a 1A maximum load current condition. The chosen MOSFET Q1 is CSD16401Q5. From the MOSFET datasheet, it specifies a 1.5V typical threshold voltage (Vgs,th) for turn-on. The absolute maximum rated gate-to-source voltage (Vgs) is specified as 16V, therefore we must limit the gate voltage to less than 16V. In order to provide sufficient design margin an 8.2V nominal zener voltage is selected. The chosen D1 zener diode is BZX84WC8V2, as shown in Figure 6-5. Similar to the voltage regulation application example above, maximum power dissipation should be calculated to ensure the package rating is not exceeded.
Figure 6-5 MOSFET Gate Overvoltage Clamping Final
Circuit