SLVAG01 February   2025 ADC12DJ5200RF

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 23 to 6dB Reasons Why
  6. 3Summary
  7. 4References

Abstract

One common question received from customers using an RF ADC, particularly when developing a passive analog frontend design, for example, using a balun or transformer to couple to the ADCs analog input pins, is: why is there a resistive 3 to 6db attenuation network between the balun and ADC? This creates a lot of signal loss! What is the purpose of this three-resistor network? Six actually, since the input is differential.