SLVAG21 April 2026 TPS61381-Q1
The selection the supercapacitor for the backup operation is majorly dependent on output load requirements, the backup duration and the internal resistance of the supercapacitor in question. The working schematic during the backup and boost mode operation is shown in Figure 2-4.
Figure 2-4 Effective Discharge During Boost Mode.Depending on the required backup time and backup power, the following equation calculates the minimum required value of the backup capacitor as given where:
However, VCL is greatly affected by supercap internal resistance Rin. The VCL must be calculated by Equation 2
Where:
Supercap internal resistance is usually 5-10 times larger than the IC MOSFET Rdson. So, efficiency mainly depends on the loss on internal resistance. The effect of the internal resistance on the backup boost operation can be calculated. See Automotive E-Latch Systems Design Guideline Using TPS61383 for detailed calculations.