SLVAG21 April 2026 TPS61381-Q1
Figure 3-3 shows the backup action of the system in play. If the mains supply fails, the TPS61381 converter immediately starts regulating the system voltage to the programmed output voltage. The supercapacitor is discharged and the voltage decreases slowly. When the backup capacitor voltage reaches the IC current limit or the minimum voltage of the TPS61381 (around 1V), the converter stops operating and the system voltage decreases to zero.
Figure 3-3 Backup Operation with Vbub=5.4V, Vout=12VIn this scope plot, the backup time is approximately 200ms. Larger backup capacitor values result in a longer backup time, in accordance with the previous equation described in section 2.3.2.