SLVS052J April 1988 – September 2026 TL594
PRODUCTION DATA
Make all of the power (high current) traces as short and direct as possible, while trying to maximize trace width for the appropriate current carrying capability. It is good practice on a standard PCB board to make the traces an absolute minimum of 15mils (0.381mm) per ampere. The inductor, output capacitors, and output diode must be as close to each other possible. This helps reduce the EMI the power traces radiate due to the high switching currents through the power traces. This also reduces lead inductance and resistance as well, which in turn reduces noise spikes, ringing, and resistive losses that produce voltage errors.
Closely connect together the grounds of the IC, input capacitors, output capacitors, and output diode (if applicable) directly to a ground plane. Have a ground plane on both sides of the PCB. This reduces noise as well by reducing ground loop errors as well as by absorbing more of the EMI the inductor radiates. For multi-layer boards with more than two layers, use a ground plane to separate the power plane (where the power traces and components are) and the signal plane (where the feedback and compensation and components are) for improved performance.
On multi-layer boards, using vias is required to connect traces and different planes. It is good practice to use one standard via per 200mA of current if the trace requires conduct to a significant amount of current from one plane to the other. Arrange the components so that the switching current loops curl in the same direction. Due to the way switching regulators operate, there are two power states. One state when the switch is on and one when the switch is off. During each state there is a current loop the power components make that are currently conducting. Place the power components so that during each of the two states the current loop is conducting in the same direction. This prevents magnetic field reversal the traces between the two half-cycles and reduces radiated EMI causes