SLVSAI3D September 2010 – May 2025 TPS736-Q1
PRODUCTION DATA
The NMOS pass element of the TPS736xx-Q1 provides inherent protection against current flow from the output of the regulator to the input when the gate of the pass device is pulled low. To ensure that all charge is removed from the gate of the pass element, the EN pin must be driven low before the input voltage is removed. If this is not done, the pass element can be left on due to stored charge on the gate.
After the EN pin is driven low, no bias voltage is needed on any pin for reverse current blocking. The reverse current is specified as the current flowing out of the IN pin due to voltage applied on the OUT pin. There is additional current flowing into the OUT pin due to the 80kΩ internal resistor divider to ground (see Figure 6-1 and Figure 6-2).
For the TPS73601, reverse current can flow when VFB is more than 1V above VIN.