SLVSGI9B October 2022 – July 2024 DRV8411A
PRODUCTION DATA
In the parallel bridge interface, the DRV8411A device is configured to drive a higher current brush DC (BDC) motor by connecting the driver outputs in parallel to reduce the RDS(on) by a factor of two. Figure 8-3 shows an example of how to connect the pins on the device. To use parallel bridge interface operation, connect AIN1 and BIN1 to the same control signal, IN1, and connect AIN2 and BIN2 to the same control signal, IN2. Similarly, connect AOUT1 and BOUT1 to the same output node, OUT1, and connect AOUT2 and BOUT2 to the same output node, OUT2.
This mode can deliver the full functionality of the BDC motor control with all four modes (forward, reverse, coast, and brake mode). Table 8-4 shows the control interface states in parallel mode.
| IN1 (AIN1) | IN2 (AIN2) | OUT1 (AOUT1 & BOUT1 | OUT2 (AOUT2 & BOUT2) | DESCRIPTION |
|---|---|---|---|---|
| 0 | 0 | High-Z | High-Z | Coast; H-bridge disabled to High-Z, automatic low-power sleep mode entered after 1ms) |
| 0 | 1 | L | H | Reverse (Current OUT2 → OUT1) |
| 1 | 0 | H | L | Forward (Current OUT1 → OUT2) |
| 1 | 1 | H | H | Brake; high-side slow decay |