SLVSH72B December   2023  – October 2026 TPS281C100

PRODUCTION DATA  

  1.   1
  2. 1 Features
  3. 2 Applications
  4. 3 Description
  5. 4 Device Options
  6. 5 Pin Configuration and Functions
  7. 6 Specifications
    1. 6.1 Absolute Maximum Ratings
    2. 6.2 ESD Ratings
    3. 6.3 Recommended Operating Conditions
    4. 6.4 Thermal Information
    5. 6.5 Electrical Characteristics
    6. 6.6 SNS Timing Characteristics
    7. 6.7 Switching Characteristics
    8. 6.8 Typical Characteristics
  8. 7 Parameter Measurement Information
  9. 8 Detailed Description
    1. 8.1 Overview
    2. 8.2 Functional Block Diagram
    3. 8.3 Device Functional Modes
    4. 8.4 Working Mode
    5. 8.5 Feature Description
      1. 8.5.1 Accurate Current Sense
        1. 8.5.1.1 High Accuracy Sense Mode
      2. 8.5.2 Programmable Current Limit
        1. 8.5.2.1 Short-Circuit and Overload Protection
        2. 8.5.2.2 Capacitive Charging
      3. 8.5.3 Inductive-Load Switching-Off Clamp
      4. 8.5.4 Inductive Load Demagnetization
      5. 8.5.5 Full Protections and Diagnostics
        1. 8.5.5.1 Open-Load Detection
        2. 8.5.5.2 Thermal Protection Behavior
        3. 8.5.5.3 Undervoltage Lockout (UVLO) Protection
        4. 8.5.5.4 Reverse Polarity Protection
          1. 8.5.5.4.1 Method 1
          2. 8.5.5.4.2 Method 2 (GND Network Protection)
        5. 8.5.5.5 Protection for MCU I/Os
        6. 8.5.5.6 Diagnostic Enable Function
        7. 8.5.5.7 Loss of Ground
  10. 9 Application and Implementation
    1. 9.1 Application Information
    2. 9.2 Typical Application
      1. 9.2.1 Design Requirements
        1. 9.2.1.1 IEC 61000-4-4 EFT
        2. 9.2.1.2 IEC 61000-4-5 Surge
      2. 9.2.2 Detailed Design Procedure
        1. 9.2.2.1 Selecting RILIM
        2. 9.2.2.2 Selecting RSNS
    3. 9.3 Power Supply Recommendations
    4. 9.4 Layout
      1. 9.4.1 Layout Guidelines
        1. 9.4.1.1 EMC Considerations
      2. 9.4.2 Layout Example
        1. 9.4.2.1 DNT Layout Without a GND Network
      3. 9.4.3 Thermal Considerations
  11. 10Device and Documentation Support
    1. 10.1 Receiving Notification of Documentation Updates
    2. 10.2 Support Resources
    3. 10.3 Trademarks
    4. 10.4 Electrostatic Discharge Caution
    5. 10.5 Glossary
  12. 11Revision History
  13. 12Mechanical, Packaging, and Orderable Information

Capacitive Charging

Capacitive Charging Circuit shows the typical setup for a capacitive load application and the internal blocks that function when the device is used. Note that all capacitive loads has an associated "load" in parallel with the capacitor that is described as a resistive load but in reality it can be inductive or resistive.

TPS281C100 Capacitive Charging
                    Circuit Figure 8-7 Capacitive Charging Circuit

The first thing to check is that the nominal DC current, INOM, is acceptable for the TPS281C100 device. This can easily be done by taking the RθJA from the Thermal Section and multiplying the RON of the TPS281C100 and the INOM with it, add the ambient temperature and if that value is below the thermal shutdown value the device can operate with that load current. For an example of this calculation see the Applications Section.

The second key care about for this application is to make sure that the capacitive load can be charged up completely without the device hitting thermal shutdown. This is because if the device hits thermal shutdown during the charging, the resistive nature of the load in parallel with the capacitor starts to discharge the capacitor over the duration the TPS281C100 is off. Note that there are some application with high enough load impedance that the TPS281C100 hitting thermal shutdown and trying again is acceptable; however, for most applications the system must be designed so that the TPS281C100 does not hit thermal shutdown while charging the capacitor.

With the current clamping feature of the TPS281C100, capacitors can be charged up at a lower inrush current than other high current limit switches. This lower inrush current means that the capacitor takes a little longer to charge all the way up. However, to minimize this longer charge time during startup, TPS281C100A implements an inrush current handling feature described in Figure 8-8. When the EN pin goes high to turn on the high side switch, the device defaults its current limit threshold to ILIM_STARTUP for a duration of ILIM_STARTUP_DELAY. During this delay period, a capacitive load can be charged at a higher rate than what typical ICL would allow and FAULT is masked to prevent unwanted Fault triggers. After ILIM_STARTUP_DELAY, the current limit default back to ICL and Fault works normally.

TPS281C100 Inrush Current
                    Handling Figure 8-8 Inrush Current Handling

The initial inrush current period when the current limit is higher enables two different system advantages when driving loads:

  • Enables higher load current to be supported for a period of time of the order of milliseconds to drive high inrush current loads like incandescent bulb loads.
  • Enables fast capacitive load charging. In some situations, it is best to charge capacitive loads at a higher current than the DC current to confirm quick supply bring up. This architecture allows a module to quickly charge a capacitive load using the initial higher inrush current limit and then use a lower current limit to reliably protect the module under overload or short circuit conditions.
TPS281C100 Auto-retry Behavior Before
                    ILIM_STARTUP_DELAY Figure 8-9 Auto-retry Behavior Before ILIM_STARTUP_DELAY
TPS281C100 Auto-retry Behavior After
                    ILIM_STARTUP_DELAY Figure 8-10 Auto-retry Behavior After ILIM_STARTUP_DELAY

While in current limiting mode, at any level, the device has a high power dissipation. If the FET temperature exceeds the over-temperature shutdown threshold, the device turns off just the channel that is overloaded. After cooling down, the device retries. If the device is turning off prematurely on start-up, it is recommended to improve the PCB thermal layout, lower the current limit to lower power dissipation, or decrease the inrush current (capacitive loading).

For more information about capacitive charging with high side switches see the How to drive Capacitive loads application note. This application note has information about the thermal modeling available along with quick ways to estimate if a high side switch can charge a capacitor to a given voltage.