SLVSHR9A December 2024 – July 2025 TPS25984B
PRODUCTION DATA
The TPS25984Bx implements undervoltage lockout on VIN in case the applied voltage becomes too low for the system or device to properly operate. The undervoltage lockout has a default internal threshold of VUVPIN on VIN. Alternatively, the UVLO comparator on the EN/UVLO pin allows the undervoltage protection threshold to be externally adjusted to a user defined value. Figure 7-1 and Equation 1 show how a resistor divider can be used to set the UVLO set point for a given voltage supply.
Figure 7-1 Adjustable Undervoltage ProtectionThe EN/UVLO pin implements a bi-level threshold.