SLVSI15A March 2025 – December 2025 TPSM8287B15 , TPSM8287B30
PRODMIX
During initialization, the device reads the state of the VSETx pins and selects the default output voltage according to Table 7-2. Note that the VSETx pins also select the I2C target address of the device and the setting of the VRANGE bits located in register CONTROL2. The VSETx pins are only read during a power cycle of VIN or by setting RESET = 1 through the I2C interface. Changing the configuration after VIN is present does not affect the content of the registers or the I2C address. Make sure that there is no stray current path connected to the VSETx pins and that the parasitic capacitance between the VSETx pins and GND is less than 100pF. For proper operation, the input voltage needs to be at least 1.5V above the selected output voltage.
| VSET1 | VSET2 | I2C ADDRESS | TPSM8287BxxL VOUT VOLTAGE(1) | TPSM8287BxxH VOUT VOLTAGE(2) |
|---|---|---|---|---|
| GND | GND | 0x45 | 400mV | 800mV |
| GND | 47kΩ to GND | 0x44 | 425mV | 850mV |
| GND | 47kΩ to VIN | 0x47 | 450mV | 900mV |
| GND | VIN | 0x46 | 475mV | 950mV |
| 47kΩ to GND | GND | 0x45 | 500mV | 1000mV |
| 47kΩ to GND | 47kΩ to GND | 0x44 | 525mV | 1050mV |
| 47kΩ to GND | 47kΩ to VIN | 0x47 | 550mV | 1100mV |
| 47kΩ to GND | VIN | 0x46 | 575mV | 1150mV |
| 47kΩ to VIN | GND | 0x45 | 600mV | 1200mV |
| 47kΩ to VIN | 47kΩ to GND | 0x44 | 625mV | 1250mV |
| 47kΩ to VIN | 47kΩ to VIN | 0x47 | 650mV | 1300mV |
| 47kΩ to VIN | VIN | 0x46 | 675mV | 1350mV |
| VIN | GND | 0x45 | 700mV | 1400mV |
| VIN | 47kΩ to GND | 0x44 | 725mV | 1450mV |
| VIN | 47kΩ to VIN | 0x47 | 750mV | 1500mV |
| VIN | VIN | 0x46 | 775mV | 1550mV |
If the user programs new output voltage setpoints (VOUT[7:0]), output voltage range (VRANGE[1:0]), or soft-start time (SSTIME[1:0]) settings when the device has already begun the soft-start sequence, the device ignores the new values until the soft-start sequence is complete. The output voltage ramps up to the target value set by the VSETx pins, before ramping up or down to any new value programmed to the device over the I2C interface. When changing VOUT[7:0], VRAMP[1:0], or SSTIME[1:0] while EN is low, the device uses the new values the next time the device is enabled.