SLVSI15B March 2025 – October 2026 TPSM8287B15 , TPSM8287B30
PRODMIX
The following subsections describe how to calculate the external components required to meet the specified transient requirements of a given application. The calculations include the worst-case variation of components and use the RMS method to combine the variation of uncorrelated parameters.
See TPSM8287B-COMPONENT-CALCULATOR for a spreadsheet component calculator with the following calculations.