SLVSI89A March 2026 – June 2026 TPS63820
PRODUCTION DATA
Ti recommends to use the TPS63820 and TPS638201 devices with 0.47µH inductor. For high efficiencies, use an inductor with a low DC resistance (DCR) and low core losses.
The saturation current of the inductor must be greater than the maximum inductor current in the application. To include sufficient margin for worst-case and transient operating conditions, use an inductor with saturation current that is at least 20% higher than the maximum inductor current in the application. The maximum current in the inductor occurs when the device operates in boost mode and the following is true:
To calculate the maximum inductor current, first use Equation 1 to calculate the maximum duty cycle during boost operation (which is when the maximum inductor current occurs).

where
Next, use Equation 2 to calculate the maximum inductor current.

where
To include enough margin for transient conditions, use an inductor with a saturation current rating at least 20% higher than the calculated maximum current.