PCB layout is a critical portion of good
power supply design. There are several paths that conduct high slew-rate currents or
voltages that can interact with stray inductance or parasitic capacitance to generate noise
and EMI or degrade the power supply performance.
- Bypass the VIN pin to GND with a low-ESR
ceramic bypass capacitor with a high-quality dielectric to help eliminate these problems.
Place CIN as close as possible to the LM5168E VIN and GND pins. Grounding for both the input and output capacitors must
consist of localized top-side planes that connect to the GND pin and GND PAD.
- Minimize the loop area formed by the input
capacitor connections to the VIN and GND pins. The input capacitor is part of the buck
converter high di/dt current loop. The high di/dt current, together with excessive
parasitic inductance between the IC and the input capacitor, can result in excessive
voltage ringing on the SW node of the IC. The placement of the input capacitor on the
board is critical for minimizing the parasitic inductance in the high di/dt loop and
accordingly minimizing the SW node ringing at each switching. For designs targeting the
maximum operating voltage of the regulator, make sure the ringing on the SW node does not
exceed the absolute maximum rating of the device. The SW node voltage ringing is a
function of how well the input capacitor is positioned with respect to the IC. Refer to
the PCB layout example in Figure 8-28 for proper placement of the input capacitors.
- Locate the inductor close to the SW pin.
Minimize the area of the SW trace or plane to prevent excessive capacitive coupling.
- Tie the GND pin directly to the power pad
under the device and to a heat-sinking PCB ground plane.
- Use a ground plane in one of the middle
layers as a noise shielding and heat dissipation path.
- Have a single-point ground connection to the
plane. Route the ground connections for the feedback, and enable components to the ground
plane. This action prevents any switched or load currents from flowing in analog ground
traces. If not properly handled, poor grounding results in degraded load regulation or
erratic output voltage ripple behavior.
- Make VIN, VOUT, and ground
bus connections as wide as possible. This guidelines reduces any voltage drops on the
input or output paths of the converter and maximizes efficiency.
- Minimize the trace length to the FB pin. Place
both feedback resistors, RFB1 and RFB2, close to the FB pin. Place
CFF (if used) directly in parallel with RFB1. If output setpoint
accuracy at the load is important, connect the VOUT sense at the load. Route
the VOUT sense path away from noisy nodes and preferably through a layer on the
other side of a grounded shielding layer.
- Note that the RT pin is sensitive to
noise. Therefore, locate the RT resistor as close as possible to the device and
route with minimal lengths of trace. The parasitic capacitance from RT to GND must not
exceed 20pF.
- Provide adequate heat sinking for the
LM5168E to keep the junction temperature
below 150°C. For operation at full rated load, the top-side ground plane is an important
heat-dissipating area. Use an array of heat-sinking vias to connect the exposed pad to the
PCB ground plane. If the PCB has multiple copper layers, these thermal vias must also be
connected to inner layer heat-spreading ground planes.