SLVSJN6 October 2026 ADC168M102R-SP
PRODUCTION DATA
As with special mode II, this device also offers a special read mode for mode IV. In this mode, as shown in Figure 6-10, both data results of a conversion are read by triggering a single RD pulse. In this case, set the SR bit in the CONFIG register to 1. The CONVST and RD pins are still tied together, but are issued every 40 CLOCK cycles instead of 20. Make sure the RD signal in this mode is no longer than one clock cycle to avoid output data corruption.
Data are available on the SDOA pin, accordingly.
If auto-sleep power-down mode is enabled, as shown in Figure 6-10, the conversion results are presented during the next conversion.
Use this mode for fully- or pseudo-differential inputs (in pseudo-differential mode, the sequencer controls the input multiplexer). Channel information is available if the CID is 0 in fully differential mode only (CID is forced to 1 in pseudo-differential mode).
The internal FIFO is available in this mode; when used, a single read pulse allows all stored conversion data to be read. Make sure the FIFO is completely filled when used for the first time to provide proper functionality.