Low-noise circuit design requires careful
analysis of all noise sources. In many cases, external noise sources can dominate; consider
the effect of source resistance on overall op-amp noise performance. Total noise of the
circuit is the root-sum-square combination of all noise components.
The resistive portion of the source impedance
produces thermal noise proportional to the square root of the resistance. The source
impedance is typically fixed; consequently, select op amp and the feedback resistors that
minimize the respective contributions to the total noise.
Figure 7-1 shows the noninverting op-amp circuit configurations with gain. Figure 7-2 shows the inverting op-amp circuit configurations with gain. In circuit configurations
with gain, the feedback network resistors also contribute noise. In general, the current
noise of the op amp reacts with the feedback resistors to create additional noise
components. However, the low current noise of the OPAx486 means
that the current noise contribution can be ignored.
The feedback resistor values can generally be
chosen to make these noise sources negligible. Low impedance feedback resistors load the
output of the amplifier. The equations for total noise are shown for both
configurations.
For additional
resources on noise calculations, visit TI Precision
Labs.
Figure 7-1 Noise Calculation
in Noninverting Gain Configurations Equation 1.
Equation 2.
Equation 3.
Equation 4.
Equation 5.
Equation 6.
where
- eN is the voltage noise
spectral density of the amplifier. For the OPAx486,
en = 9.2nV/√Hz at 1kHz)
- iN is the current noise spectral density of the
amplifier. For the OPAx486, in =
200fA/√Hz at 1kHz)
- eo is the total noise
density
- eS is the thermal noise of
RS
- eR1 ||
R2 is the thermal noise of R1 || R2
- kB is the Boltzmann
constant
- T(K) is the temperature in kelvins
Figure 7-2 Noise Calculation
in Inverting Gain Configurations Equation 7.
Equation 8.
Equation 9.
Equation 10.
Equation 11.
where
- eN is the voltage noise spectral density of the
amplifier. For the OPAx486, en =
9.2nV/√Hz at 1kHz)
- iN is the current noise spectral density of the
amplifier. For the OPAx486, in =
200fA/√Hz at 1kHz)
- eo is the total noise density
- eS is the thermal noise of RS
- e(R1 + RS)
|| R2 is the thermal noise of (R1 + RS) ||
R2
- kB is the Boltzmann constant
- T(K) is the temperature in kelvins