SLVSL58 September 2026
ADVANCE INFORMATION
The EVM uses an I2C-compatible interface for serial communication. Each target device on an I2C bus must have a unique address. The EVM uses address 0x48h to communicate with the ADS111C04 and address 0x49h to communicate with the ADS111C02. Communication on the I2C bus always takes place between two devices: one acting as the controller and the other as the target. Both the controller and target can receive and transmit data, but the target can only read or write under the direction of the controller. The EVM always acts as the I2C target devices.