SLVSLR3A August 2026 – October 2026 TMUX5508 , TMUX5509
PRODUCTION DATA
Off isolation is defined as the voltage at the drain pin (D, DA, or DB) of the TMUX550x when a 1VRMS signal is applied to the source pin (Sx, SxA, or SxB) of an off-channel. Figure 7-8 shows the setup used to measure off isolation. Use Equation 2 to compute off isolation.
Figure 7-8 Off Isolation Measurement
Setup