Add a decoupling capacitor from
VCC to GND. The capacitor needs to be placed physically close to
the device and electrically close to both the VCC and GND pins. An
example layout is shown in the Layout section.
Verify that the capacitive load
at the output is ≤ 50pF. Low load capacitance can be accomplished by providing
short, appropriately sized traces from the SN74LVC1G135B-Q1 to the receiving device.
Verify that the resistive load at
the output is larger than (VCC / IO(max))Ω. Never violate
the maximum output current from the Absolute Maximum Ratings. Most CMOS
inputs have a resistive load measured in MΩ; much larger than the minimum
calculated previously.