SLVUBV0A March 2020 – September 2020 TPS55288
The TPS55288EVM board can be enabled to work by the following steps:
Step 1: Set JP1 to the ON position. Turn on the power supply.
Step 2: Open the TPS55288EVM GUI.
Step 3: Click the auto connect button on the slave address widget (Figure 4-2). It will automatically check for slave addresses (0x74, 0x75) and connect the GUI with device. Once after connection, GUI will read all the 8 registers and show a notification (Figure 4-3).
Figure 4-2 GUI Auto Connect Button
Figure 4-3 GUI Auto Connect NotificationStep 4: Click the start button. It will show the GUI user interface of TPS55288EVM-053 (Figure 4-4).
Figure 4-4 GUI User Interface of TPS55288EVM-053Step 5: Click the Enable button (Figure 4-5). The default output voltage is 5 V.
Figure 4-5 ENABLE ButtonStep 6: Set the output voltage, current limit point, etc. according to the design target. If the maximum load current is ≥ 5 A, untick the ‘Enable Current Limit’ check box or increase the current limit value (Figure 4-6).
Figure 4-6 Output Current Limit Point Setting