SLVUCK7A november 2022 – july 2023
CM filters for both commercial (Class A) and residential (Class B) environments typically have limited Y-capacitance due to touch-current safety requirements and thus require large-sized CM chokes to achieve the requisite attenuation. This ultimately results in filter designs with bulky, heavy and expensive passive components. The deployment of active filter circuits enable more compact filters for next-generation power conversion systems.
Figure 3-2 presents typical schematics of equivalent single-phase passive and active filter designs. Terminals designated L, N and PE refer to Live, Neutral and Protective Earth, respectively. Comparing the passive and active circuits in Figure 3-2, the CM inductance of chokes LCM1 and LCM2 each reduces by a factor of four to six times by virtue of the higher effective Y-capacitance with the TPSF12C1 circuit.
The AEF circuit uses a capacitive multiplier circuit in place of the two Y-capacitors normally placed between the CM chokes in a conventional two-stage passive filter design – see CY5 and CY6 in Figure 3-2. The TPSF12C1 senses the high-frequency CM disturbance on the two power lines using a set of Y-rated sense capacitors and injects a noise-canceling current back into the power lines using a Y-rated inject capacitor.
The X-capacitors placed between the two CM chokes provides a low-impedance path between the power lines from a CM standpoint, typically up to low-MHz frequencies. This allows current injection onto one power line (neutral in this case) using only one inject capacitor.
The advantages of AEF with the TPSF12C1 summarize as: