The TPS61381QEVM board can be enabled by
following the steps below:
- Set the EVM hardware as described in step 1-6 in Section 2.2.1. Turn on the power
supply.
- Open the TPS61381QEVM GUI.
- Click the connect button on the bottom bar, as shown in Figure 3-2. After the GUI and device are connected, the GUI reads all registers and
shows a notification.
- Click the Start button and the GUI
automatically turns on to the Configuration Screen (see Figure 3-3). The TPS61381 is set to boost enable by default. The default output
voltage is 6.2V. Set the boost mode output voltage, current limit point, and so forth
according to the design target.
- Click the
Charger Settings button and switch to Charger Settings Sheet (see Figure 3-4). The charger is set to Li-ion mode by default. Set the charger mode
battery type, cell number, CC current, and so forth according to the design target.
- Click the SOH Settings button and
switch to the SOH Settings Sheet (see Figure 3-5). Set the SOH discharge current, AVI pin output ratio, AVI output, and
so forth according to the design target.