The EVM hardware is designed and kitted to
simplify setup and begin spinning motors. The EVM comes with the jumpers placed at
the appropriate location in the headers. The location of the jumpers, also called
shunts, are shown in Figure 3-1.
Note: Before using the EVM, check that the shunt
location matches the location shown in
Figure 3-1.
Before connecting the EVM to the GUI software, follow these steps:
- Make sure all the jumpers are populated on J1 and
J2 if using the GUI with the EVM controller. If users are not using the GUI and
TI firmware, then users can remove all the jumpers from J2 except the bottom
most jumper DVDD. Users can remove the DVDD jumper if the DVDD voltage is
supplied externally and not from the onboard MCU.
- If using the EC driver, then make sure J23 is set
to the desired position.
- Connect the micro-USB cable to micro-USB
receptacle in the XDS110 section. LED2 illuminates.
- Provide VBAT voltage through VBAT connector.
- Set up is now complete. See Figure 3-5 for setup image.