SLVUD70 July 2025
The Registers section provides an overview of the internal register map, and includes basic interfaces for each PMIC register.
Figure 3-6 TPS65036x-Q1 GUI Register Map PageThe register table displays each register name, address, last known value from the PMIC, and corresponding bit values. Selecting a title or bit fields in the table updates the Field View column on the right side of the GUI. The Field View displays the individual fields contained within the associated register address. Within the Register page, selecting a blue icon containing a question mark (?) expands additional descriptions, if available. Close the expanded description views by selecting the red (x) icon.
The Register page polls the device periodically using the Auto Read feature in the top-right corner. Disable automatic reads by changing the Auto Read setting to Off and perform manual read instructions using the Read Register, to read the currently selected register, and Read All Registers buttons.
The Write Mode button at the top right of the register map indicates how the registers are written as the user interacts with the Register page. With Immediate enabled, any update to the Register page is automatically sent to the PMIC. If Immediate is disabled, then writes are only sent upon selecting either Write Register or Write All Registers. After each write, the Register page automatically reads the affected register address to confirm the latest value in the device.