SLVUDA9B October   2025  – October 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specifications
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 I/O Information
    2. 2.2 Jumper Information
    3. 2.3 Equipment
    4. 2.4 Hardware Setup
  9. 3Software
    1. 3.1 Software Setup
    2. 3.2 Test Procedure
      1. 3.2.1 Initial Power Up
      2. 3.2.2 I2C Register Setup
      3. 3.2.3 Forward/Charge/Sink Mode Verification
      4. 3.2.4 Reverse/OTG/Source Mode Verification
      5. 3.2.5 Helpful Tips
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
      1. 4.2.1 PCB Layout Guidelines
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1.     Trademarks
  12. 6Revision History

Software Setup

BQSTUDIO

If using BQSTUDIO and either the EV2400 or EV2500 communication box, use the following steps to set up the EVM testing software:

  1. Connect the EV2400 or EV2500 to the PC with BQSTUDIO installed on it using the USB cable. If using the EV2500, the USB-A to USB-C cable is not included but is required to connect the EV2500 to the PC.
  2. Connect the EV2400 or EV2500 to the EVM using the 4-pin Molex cable.
  3. Launch BQSTUDIO and select "Charger" from the first splash screen.
  4. On the second splash screen, select Charger_1_00-BQ25692-Q1 from the list of available BQZ files.
  5. On the last screen, while you can use either the Default View tab or the Field View tab, the Field View gives a more concise view.

TI-CHARGER-GUI

If using TI-CHARGER-GUI and USB2ANY communication box, use the following steps to set up the EVM testing software:

  1. Connect the USB2ANY box to the EVM using the 10-pin ribbon cable.
  2. Launch TI-CHARGER-GUI from the website.
  3. Either type in search box or scroll down to find BQ25692-Q1.
  4. Find the page of interest using the icons on the left of the page:
    1. rocket - quick start with most common registers needed to start battery charging
    2. IC - entire chip level settings like EN_CHG, EN_REV, EN_HIZ, EN_PFM, etc
    3. plug - all forward/charge mode register settings
    4. lightning bolt - all reverse/OTG mode register settings
    5. bell - status and fault registers (fault registers clear after being read)