SLVUDE5 September 2025
The TMUX48XXDSGDDF-EVM has seven 3-pin headers to control the power supply connection, the control inputs, the sources and drains. The following is a description of each header.
Header J1 connects the VDD pin to either the external power or to ground via a jumper. If Header J1 is not connected, then the devices supply is left floating. Figure 2-1 shows header J1.
Header J6 connects the SEL1 pin to either VDD or ground by a jumper. If Header J6 is not connected, then the devices SEL1 pin is left floating.
Header J7 connects the SEL2 pin to either VDD or ground via a jumper. If Header J7 is not connected, then the devices SEL2 pin is left floating.
Header J2 connects the D1 pin to either VDD or ground by a jumper. If Header J2 is not connected, then the devices D1 pin is left floating.
Header J3 connects the D2 pin to either VDD or ground via a jumper. If Header J3 is not connected, then the devices D2 pin is left floating.
Header J4 connects the S1 pin to either VDD or ground by a jumper. If Header J4 is not connected, then the devices S1 pin is left floating.
Header J5 connects the S2 pin to either VDD or ground by a jumper. If Header J5 is not connected, then the devices S2 pin is left floating.
Figure 2-1 Header J1 : J1-1(GND), J1-2(Connection to device VDD), J1-3 (V_EXT)
Figure 2-2 Header J6 : J6-1(GND), J6-2(Connection to device SEL1), J6-3 (VDD)
Figure 2-3 Header J7 : J7-1(GND), J7-2(Connection to device SEL2), J7-3 (VDD)
Figure 2-4 Header J2 : J2-1(VDD), J2-2(Connection to device D1), J2-3 (GND)
Figure 2-5 Header J3 : J3-1(VDD), J3-2(Connection to device D2), J3-3 (GND)
Figure 2-6 Header J4 : J4-1(GND), J4-2(Connection to device S1), J4-3 (VDD)
Figure 2-7 Header J5 : J5-1(GND), J5-2(Connection to device S2), J5-3 (VDD)The logic headers J6(SEL1) and J7(SEL2) can be used to control both the TMUX4821 and TMUX4819. The TMUX4819 has an EN pin which can be controlled by SEL2 and the SEL pin to be controlled by SEL1.
Figure 2-8 TMUX48XXDSGDDF-EVM TMUX4821 Truth Table
Figure 2-9 TMUX48XXDSGDDF-EVM TMUX4819 Truth Table