SLVUDG8 December 2025
Common-mode and differential input filtering can be applied to the circuit using C7, C8, C10. These components are unpopulated by default. When selecting component values for the capacitors, the recommendation is to make C8 approximately ten times larger than C7 and C10. Analog Engineer's Calculator tool, can be used to calculate the needed resistor and capacitor values for a given cutoff frequency. Note that any capacitor and resistors selected must be rated for the inputs being applied.