SLVUDH7 December 2025
The SNSR-DUAL-ADC-EVM default settings configure ADC1 to measure the output signals of a resistive bridge. However, the user can configure the channels to measure general purpose sensor signals. Figure 5-4 shows the analog input filtering and additional circuitry connected to ADC1.
AIN2 and AIN3 form a differential pair that measures the input signals between SIGNAL+ and SIGNAL-. The default EVM settings configure AIN4 and AIN5 as the reference between SENSE+ and SENSE-. The user can also configure AIN4 and AIN5 as a differential pair to measure input signals. The default EVM settings configure AIN1 as the excitation source return path from an external bridge circuit. However, AIN1 can also be used as a single-ended measurement input when resistor R12 is removed.
ADC1 supports resistive bridge, thermocouple, 3- and 4-wire resistance temperature detectors (RTDs), and generic voltage and current input measurements. See Analog Sensor Connections for additional details regarding how to connect sensors to the SNSR-DUAL-ADC-EVM board.
The ADC1 analog inputs include first-order resistor-capacitor filters that limit aliasing and noise effects. The differential pairs include an additional common-mode capacitor that filters common-mode noise. Equation 3 shows the calculation for the differential cut-off frequency. Equation 4 shows the calculation for the common-mode cut-off frequency.