SLVUDH7 December 2025
Figure 5-6 shows the sensor excitation circuitry. Header J4 functions as both an output and an input to the EVM. This header supports multiple sensor excitation sources, including VDD, REFOUT_ADC1, and IDAC_ADC1. EXC- completes the bridge connection to ground through the TMUX1219, which acts as a low-side bridge switch. The MSPM0G1507 controls the low-side bridge switch to either provide the bridge excitation with a path to ground or disconnect the bridge for power savings. Refer to Section 6.3.2.6 for additional information regarding how to operate the low side bridge switch.
In a current excitation bridge circuit, replace the 0Ω resistor R12 with a bias resistor to establish a valid common mode voltage for the bridge output. Additionally, this bias resistor provides a return path for the excitation current source.