The TPS25752AEVM fully integrates and
seamlessly connects to the
LM251772EVM-PD. Both evaluation boards can be connected together as seen
below in
Figure 2-3:
Note that in this configuration the I2C address of the LM251772EVM-PD must be set
appropriately in the USBCPD Application Customization Tool. The ADDR header (JP9) on the
LM251772EVM-PD must be set to the corresponding address that was configured in the
customization tool. Setting the JP9 jumper to Pin1 and Pin2 position sets the I2C
address to 0x6A and setting the jumper to the Pin2 to Pin3 position sets it to 0x6B.