SLVUDP6 June 2026
The JP1 jumper is used to configure SCL for the I2C interface. By default, this jumper is left open and the device uses the USB2ANY adapter internal pull up. Set this jumper to H position to enable pull-up circuit on the EVM. Put this jumper in the L position to disable the SCL.
The JP2 jumper is used to enable SDA for the I2C interface. By default, this jumper is left open and the device uses the USB2ANY adapter internal pull up. Set this jumper to H position to enable pull-up circuit on the EVM. Put this jumper in the L position to disable the SDA.