SLYT854 May   2024 ADS8900B , OPA2320

 

  1.   1
  2. 1Introduction
  3. 2The impact of the voltage reference on ADC noise
  4. 3The impact of the voltage reference on THD
  5. 4How voltage reference noise and THD affect the ENOB
  6. 5How voltage reference noise affects noise-free resolution
  7. 6Conclusion

How voltage reference noise affects noise-free resolution

While ENOB valuably represents the resolution of your ADC output, it does not account for DC performance. To understand the resolution implications of noise from a DC input to your ADC, consider finding the noise-free resolution of your circuit. Using Equation 4 you can calculate the noise-free resolution by observing the code spread in number of least-significant bits (LSB) of an ADC’s digital output while measuring a DC signal:

Equation 4. N o i s e   F r e e   R e s o l u t i o n = N   -   l o g 2 ( C o d e   S p r e a d )

To highlight the impact of reference noise on the system precision performance, my colleagues and I conducted DC code spread tests for a given signal chain using the REF70 (with 0.23ppmp-p flicker noise) and the REF50 (with 3ppmp-p flicker noise). Both the REF50 and REF70 are high-precision voltage references used with high-precision ADCs, and have differing DC characteristics. However, in this exercise, the goal was solely to compare the noise performance of these devices in a signal-chain circuit.

The design uses batteries for a stable DC source with a voltage level close to the full-scale range of the ADS8900B 20-bit SAR ADC, which captures data at 20kSPS. OPA2320 is used with a gain = 1 to drive the ADS8900B inputs. This ADC integrates the reference buffer driver; therefore, an optional reference buffer is not required. Placing a simple resistor-capacitor low-pass filter on the output of the voltage reference further lowers the noise from the voltage reference. Figure 3 shows the setup used for these tests.

 The circuit used for the
                    following noise-free resolution tests. Figure 3 The circuit used for the following noise-free resolution tests.

The signal-chain components beside the voltage reference also have flicker noise, which will be part of the final code spread. Because the signal chain remains the same with different references only, the impact on performance numbers must be from the voltage reference noise only.

High-precision systems employ data-processing techniques to improve the precision and increase the overall resolution. In this experiment, we converted the 20-bit raw data from the ADS8900B to a 24-bit length by multiplying the output by 16. Different finite impulse response (FIR) filters processed the converted 24-bit data. FIR filters are easy to implement and settle faster if there’s a change in the input values. The output data rate remains at 20kSPS, but with latency as defined by the filter characteristics.

At a 24-bit level, the noise (and thus the precision) of REF50 and REF70 are almost similar, with the overall noise dominated by the signal chain and its wide bandwidth noise. The difference in the average code value is because of the reference voltage difference – an accuracy specification that you can eliminate through calibration. These results can be seen in Figure 4 and Figure 5.

 Results with REF50 noise =
                        3ppmp-p. Figure 4 Results with REF50 noise = 3ppmp-p.
 Results with REF70 noise =
                        0.23ppmp-p. Figure 5 Results with REF70 noise = 0.23ppmp-p.

We used the Octave tool to conduct post-processing of the raw data with three different digital filters:

  • 1,024-tap moving average filter.
  • 801-tap 17Hz low-pass filter.
  • 455-tap 36Hz low-pass filter.

Figure 6 shows the filter response for these filters.

 Digital filter
                    response. Figure 6 Digital filter response.

Figure 7, Figure 8 and Figure 9 illustrate the impact of the digital filter on the code spreads.

 1,024-tap filter
                    histogram. Figure 7 1,024-tap filter histogram.
 455-tap filter
                    histogram. Figure 8 455-tap filter histogram.
 801-tap filter
                    histogram. Figure 9 801-tap filter histogram.

Using Equation 4,you can easily compare the impact of the REF50 and REF70 with each filter profile on the ADC resolution. The results from these tests are summarized in Table 1.

Table 1 Comparison of DC code spread using different filter profiles and reference devices.
Digital filter type Corner frequency (Hz) Number of taps DC code spread (LSB) Noise-free resolution (bits) DC code spread least significant bit Noise-free resolution (bits)
REF70 at 24 bits REF50 at 24 bits
No filter N/A 0 448 15.1 496 15.0
1,024 tap moving average 8 1,024 35 18.8 118 17.1
FIR No. 1 17 801 38 18.7 121 17.0
FIR No. 2 36 455 49 18.3 135 16.9

This comparison shows that in the highest precision applications, the REF70 performs better than the REF50 when calculating noise-free resolution, mostly because of the devices’ difference in flicker noise levels. The reduced code spread when using the REF70 shows that its ultra-low noise can offer nearly a 2-bit resolution advantage in high-precision applications. Additionally, we can see that using a low noise reference allows using a fast 455 tap filter while still being able to maintain a high noise free resolution. Low voltage reference flicker noise will lead to lower code spread, thus enabling higher noise-free resolution. Like the ENOB, noise is an important consideration when designing your signal chain for low noise-free resolution.