SLYT865 March 2025 LMG3422R030 , LMV797 , SN74LV1T125 , TLV713P-Q1 , TMS320F280033
I tested the proposed method on a 3.6kW totem-pole bridgeless PFC [2]. Figure 6 shows that when the AC voltage drops out, it comes back in 10ms at its peak. Channel 1 (blue) is the PFC input current waveform (IIN), while channel 2 (turquoise) is the relay on and off control signal. Figure 7 is the zoom in at relay on and off. During the AC drop period, relay Q5 remains on. CBULK continuously delivers the stored energy to the load and VOUT drops. After the AC voltage resumes, because the relay is on and VAC > VOUT, the re-rush current quickly rises. Once the re-rush current reaches a predefined current limit threshold (40A in this example), the relay turns off, and the re-rush current reduces to a very low value because of RT. The relay only remains off for 10µs, then turns on again. The re-rush current rises once again. This entire process allows the limiting of re-rush current within the M-CRPS specification while still supplying substantial current to rapidly charge CBULK. The waveform also shows that the non-re-rush current, where VAC < VOUT, is well controlled without large current spikes.
Figure 6 Re-rush current control when
the AC voltage resumes after dropout.Figure 7 shows the second re-rush current rising up with a limited slope, which occurs because the PFC input impedance – including the electromagnetic interference filter impedance and printed circuit board trace impedance – limit the current rising slope. The magnitude of the second re-rush current does not exceed the 40A threshold in this example; therefore, the relay turns off only once. If the second re-rush current also exceeds the threshold, the relay will turn off again.
Figure 7 Zoomed-in Figure 6 at the
relay on and off instant.