SLYU063A September 2024 – January 2025 TMAG5133 , TMAG5233
To use the EVM with the TI-SCB Controller, connect the EVM as shown in Figure 3-1, or connect the EVM using one of the ways described in Section 2. The TMAG5x33 output(s) trigger when a magnet is near the sensor. When the magnetic field at the sensor crosses the threshold of the device, the output turns the LED(s) on. The user can also check the output through the connector on the board.
Figure 3-1 EVM With Magnet