SLYU066 October 2023
The firmware must be flashed onto the SCB to properly communicate to the TMAG3001EVM. After flashing the SCB with the TMAG3001EVM firmware, the firmware does not have to be flashed again on the SCB as long as the firmware is not erased or replaced with the firmware for a different EVM. If the firmware is erased or replaced, then he TMAG3001EVM firmware must be flashed onto the SCB again to communicate to the TMAG3001EVM. The latest version of the firmware can be downloaded from: https://www.ti.com/tool/download/TMAG3001EVM-BSL.