SNAS894B July 2025 – December 2025 LMR60460-Q1
PRODMIX
LMR60460-Q1 features a precision enable and undervoltage lockout (UVLO) feature that enables the user to select the voltage level at which the device powers on and off based on the voltage present at the EN pin. To power on the device, the voltage across the EN pin and PGND pin must exceed the enable voltage rising threshold VEN-TH(R) (1.25V typical). After VEN-TH(R) has been crossed, and the minimum supply voltage, VINUVLO(R), have both been satisfied, the device begins the soft-start sequence described in Section 7.3.2.
The EN pin can be used to power down the device by reducing the voltage across EN pin and PGND pin below the enable input low threshold VEN-TH(F) (1V typical).
A resistor divider between VIN and PGND with the center point connected to the EN pin can be used to implement the VIN UVLO. To begin, select the input voltage at which the device turns off, choose the value of RENT, then calculate the required RENB. After RENB has been calculated, the resulting turn-on input voltage can be calculated. See Figure 7-1, Equation 1, and Equation 2 to determine the EN resistors required. If the VIN UVLO feature is not needed, the EN pin can be connected directly to VIN.
Where: