SNIA053 june 2023 TMP61-Q1
A common method of tracking critical component temperature is to capture the temperature of a heat sink contacting the device of interest, as shown in Figure 1-1. Mechanically, the sensors in these applications can either be attached to the heat sink with epoxy, a clip, or a bolt if the package permits. The equivalent thermal circuit for this method is shown in Figure 1-1, where the RϴJC(IGBT) is the thermal resistance from the junction of the insulated-gate bipolar transistor (IGBT) module to the top of the module package.
Figure 1-1 Equivalent Thermal Circuit for Heat Sink
Temperature SensingWhen using this method of temperature monitoring, the measured temperature at the sensor depends on a few key considerations: the thermistor, epoxy, and the mounting stud used for contact. The following sections of this application note explore tradeoffs and considerations when using ring lug thermistors to measure heat sink temperature.