SNLA490 March 2025 ISOM8110-Q1 , ISOM8111-Q1 , ISOM8112-Q1 , ISOM8113-Q1 , ISOM8115-Q1 , ISOM8116-Q1 , ISOM8117-Q1 , ISOM8118-Q1
The ISOM8118-Q1 has transistor output characteristics similar to a conventional transistor and can operate in active, saturation, reverse, and cutoff regions. To ensure that a low level is correctly output after the input drops below the threshold at the minimum CTR, the R2 resistance must satisfy:
where VCE(SAT) = 0.3V and CTRMIN = 295%, so that R2<1.02kΩ is calculated. In the meantime, the R2 resistance should not be too small to avoid over-current at the ISOM8118-Q1 output, so the R2 resistance should also satisfy:
The calculation yields R2>60Ω. With these considerations in mind, choosing R2 to be 1kΩ ensures that the circuit works properly while effectively avoiding any risk of over-current