SNOS611F July   1999  – March 2025 LMC6041 , LMC6042 , LMC6042-MIL , LMC6044 , LMC6044-MIL

PRODUCTION DATA  

  1.   1
  2. 1Features
  3. 2Applications
  4. 3Description
  5. 4Pin Configuration and Functions
  6. 5Specifications
    1. 5.1 Absolute Maximum Ratings
    2. 5.2 ESD Ratings
    3. 5.3 Recommended Operating Conditions
    4. 5.4 Thermal Information: LMC6041
    5. 5.5 Thermal Information: LMC6042
    6. 5.6 Thermal Information: LMC6044
    7. 5.7 Electrical Characteristics
    8. 5.8 Typical Characteristics
  7. 6Application and Implementation
    1. 6.1 Application Information
      1. 6.1.1 Amplifier Topology
      2. 6.1.2 Compensating For Input Capacitance
      3. 6.1.3 Capacitive-Load Tolerance
    2. 6.2 Typical Applications
      1. 6.2.1 Instrumentation Amplifiers
      2. 6.2.2 Low-Leakage Sample and Hold
      3. 6.2.3 Square-Wave Generator
      4. 6.2.4 AC Coupled Power Amplifier
    3. 6.3 Layout
      1. 6.3.1 Layout Guidelines
        1. 6.3.1.1 Printed-Circuit-Board Layout for High-Impedance Work
      2. 6.3.2 Layout Examples
  8. 7Device and Documentation Support
    1. 7.1 Receiving Notification of Documentation Updates
    2. 7.2 Support Resources
    3.     Trademarks
    4. 7.3 Electrostatic Discharge Caution
    5. 7.4 Glossary
  9. 8Revision History
  10. 9Mechanical, Packaging, and Orderable Information

Printed-Circuit-Board Layout for High-Impedance Work

As a general rule, any circuit that must operate with less than 1000pA of leakage current requires special layout of the printed circuit board (PCB). To take advantage of the ultra-low input current of the LMC604x, typically 150fA, an excellent layout is essential. Fortunately, the techniques used to obtain low leakages are quite simple. First, do not ignore the surface leakage of the PCB, even though the leakage current can sometimes appear acceptably low, because under conditions of high humidity, dust, or contamination, the surface leakage can be appreciable.

To minimize the effect of any surface leakage, lay out a ring of foil completely surrounding the LMC604x inputs and the terminals of capacitors, diodes, conductors, resistors, relay terminals, and anything else connected to the inputs of the op amp (see also Figure 6-14). To have a significant effect, place guard rings on both the top and bottom of the PCB. Then, connect the foil to a voltage that is at the same voltage as the amplifier inputs, because no leakage current can flow between two points at the same potential. For example, a PCB trace-to-pad resistance of 1012, which is normally considered a very large resistance, can leak 5pA if the trace is a 5V bus adjacent to the pad of the input. This leakage can cause a 250 times degradation from the actual performance of the LMC604x. However, if a guard ring is held within 5mV of the inputs, then even a resistance of 1011Ω causes only 0.05pA of leakage current. See Figure 6-10 to Figure 6-12 for typical connections of guard rings for standard op-amp configurations

LMC6041 LMC6042 LMC6044 Typical Connections of Guard
                    Rings: Inverting Amplifier Figure 6-10 Typical Connections of Guard Rings: Inverting Amplifier
LMC6041 LMC6042 LMC6044 Typical Connections of Guard
                    Rings: Noninverting Amplifier Figure 6-11 Typical Connections of Guard Rings: Noninverting Amplifier
LMC6041 LMC6042 LMC6044 Typical Connections of Guard
                    Rings: Follower Figure 6-12 Typical Connections of Guard Rings: Follower

If laying out a PCB for the sake of just a few circuits is not practical, the following technique is even better than a guard ring. Do not insert the input pin of the amplifier into the PCB at all. Instead, bend the pin up in the air, and use only air as an insulator because air is an excellent insulator. In this case, you forgo some of the advantages of PCB construction, but the advantages are sometimes well worth the effort of using point-to-point up-in-the-air wiring. Figure 6-13 shows an example of air wiring.

LMC6041 LMC6042 LMC6044 Air Wiring
Note: The input pins are lifted out of the PCB and soldered directly to components. All other pins connected to the PCB.
Figure 6-13 Air Wiring