SNOSB30Q October 2008 – March 2026 LMH6554
PRODUCTION DATA
Many application circuits have capacitive loading. As shown in Figure 7-4, amplifier bandwidth is reduced with increasing capacitive load, so parasitic capacitance must be strictly limited.
To maintain stability resistance must be added between the capacitive load and the amplifier output pins. The value of the resistor is dependent on the amount of capacitive load as shown in Figure 7-5. This resistive value is a suggestion. System testing is required to determine the desired value. Using a smaller resistor retains more system bandwidth at the expense of overshoot and ringing, while larger values of resistance reduces overshoot but also reduces system bandwidth.
Figure 7-4 Frequency Response vs Capacitive Load
Figure 7-5 Suggested ROUT vs Capacitive Load