SNOSDJ9B December 2024 – November 2025 TLV3511 , TLV3512
PRODMIX
The overdrive voltage, VOD, is the amount of input voltage beyond the reference voltage (and not the total input peak-to-peak voltage). The overdrive voltage is 100mV as shown in the above example. The overdrive voltage can influence the propagation delay (tp). The smaller the overdrive voltage, the longer the propagation delay, particularly when <100mV. If the fastest speeds are desired, TI recommends appling the highest amount of overdrive possible.
The risetime (tr) and falltime (tf) is the time from the 20% and 80% points of the output waveform.