SNVS089P July 2000 – September 2026 LM3488
PRODUCTION DATA
The LM3488 uses a current mode control scheme. The main advantages of current mode control are inherent cycle-by-cycle current limit for the switch, and simpler control loop characteristics. Paralleling power stages using current mode control is also easy as current sharing is automatic.
Current mode control has an inherent instability for duty cycles greater than 50%, as shown in Figure 6-2. In Figure 6-2, a small increase in the load current causes the switch current to increase by ΔIO. The effect of this load change, ΔI1, is:

From the above equation, when D > 0.5, ΔI1 is greater than ΔIO. In other words, the disturbance is divergent. So a very small perturbation in the load causes the disturbance to increase.
To prevent the sub-harmonic oscillations, a compensation ramp is added to the control signal, as shown in Figure 6-3.
With the compensation ramp,

Figure 6-2 Sub-Harmonic Oscillation for
D>0.5
Figure 6-3 Compensation Ramp Avoids
Sub-Harmonic OscillationThe compensation ramp has been added internally in LM3488. The slope of this compensation ramp has been selected to satisfy most of the applications. The slope of the internal compensation ramp depends on the frequency. This slope can be calculated using the formula:
In the above equation, VSL is the amplitude of the internal compensation ramp. Limits for VSL have been specified in the electrical characteristics.
To provide the user additional flexibility, a patented scheme has been implemented inside the IC to increase the slope of the compensation ramp externally, if the need arises. Adding a single external resistor, RSL(as shown in Figure 6-4) increases the slope of the compensation ramp, MC by :

In this equation, ΔVSL is equal to 40.10-6RSL. Hence,

ΔVSL versus RSL has been plotted in Figure 6-5 for different frequencies.
Figure 6-4 Increasing the Slope of the Compensation Ramp
Figure 6-5 ΔVSL vs RSL