SNVS686L March 2011 – June 2025 LMZ22005
PRODUCTION DATA
At light load the regulator will operate in discontinuous conduction mode (DCM). With load currents above the critical conduction point, it will operate in continuous conduction mode (CCM). In CCM, current flows through the inductor through the entire switching cycle and never falls to zero during the OFF-time. When operating in DCM, inductor current is maintained to an average value equaling IOUT. Inductor current exhibits normal behavior for the emulated current mode control method used. Output voltage ripple typically increases during this mode of operation.
Figure 6-2 is a comparison pair of waveforms of the showing both CCM (upper) and DCM operating modes.