SNVSCP2A March 2025 – August 2025 LP5815
PRODUCTION DATA
The LP5815 provides instant blinking via STAT control function for applications that require LED indication before controller is ready to send command. When VCC voltage is higher than VCC_UVLO and instant blinking function is not disabled (INSTABLINK_DIS = 0), the OUT0 waits 300ms blank time to start blinking after STAT being pulled high. The timing is shown in Figure 7-9.
During the 300ms blank time after STAT being pulled high:
While the LP5815 staying in INSTANT BLINKING mode:
Figure 7-10 shows the parameters of 1 cycle blinking pattern.
At the beginning, there is 500ms pause time before PWM starts ramping up. After the pause time, the PWM ramps up from 0 to 50% in 200ms, then keeps 50% for 1s. Next, PWM starts ramping down from 50% to 0 in 200ms. At last, the PWM keeps off for another 500ms pause time before the next cycle starts.
The maximum current setting for the instant blinking is 25.5mA with OUT0_DC = 0xFF, MAX_CURRENT = 0.
Figure 7-11 shows a typical application circuit that provides the instant blinking function. The STAT pin is pulled up by an external resistor to the battery voltage or bus voltage of the charger. And there is a LED connected to OUT0.
When the battery voltage drops below the charging threshold, the charger starts to work and can turn off the STAT pulling down switch. Then the LED connected to OUT0 starts blinking as long as the VCC voltage of the LP5815 is higher than the VCC_UVLO threshold, which indicates the charging status. When the battery charging is completed, the charger can turn on the STAT pulling down switch to pull down the STAT to make the LP5815 exit the instant blinking state. Then the LED stops blinking to indicate the charging is completed.