SPRAC71B February 2019 – October 2023
A generic EXTAB entry is indicated by setting bit 31 of the first word to 0. The first word has a PREL31 entry representing the address of the personality routine. The rest of the words in the EXTAB entry are data that are passed to the personality routine.

The format of the optional data is up to the discretion of the personality routine, but the length must be an integer multiple of whole 32-bit words. The unwinder calls the personality routine, passing it a pointer to the first word of optional data.