SPRAC71B February 2019 – October 2023
As a special case, if the second word of the EXIDX has the value 0x1, the EXIDX represents EXIDX_CANTUNWIND, indicating that the function cannot be unwound at all. If an exception tries to propagate through such a function, the unwinder calls abort or std::terminate, depending on the language.