SPRAC71C February   2019  â€“ March 2026

 

  1.   1
  2. 1 Introduction
    1. 1.1  ABIs for the C28x
    2. 1.2  Scope
    3. 1.3  ABI Variants
    4. 1.4  Toolchains and Interoperability
    5. 1.5  Libraries
    6. 1.6  Types of Object Files
    7. 1.7  Segments
    8. 1.8  C28x Architecture Overview
    9. 1.9  C28x Memory Models
    10. 1.10 Reference Documents
    11. 1.11 Code Fragment Notation
  3. 2 Data Representation
    1. 2.1 Basic Types
    2. 2.2 Data in Registers
    3. 2.3 Data in Memory
    4. 2.4 Pointer Types
    5. 2.5 Complex Types
    6. 2.6 Structures and Unions
    7. 2.7 Arrays
    8. 2.8 Bit Fields
      1. 2.8.1 Volatile Bit Fields
    9. 2.9 Enumeration Types
  4. 3 Calling Conventions
    1. 3.1 Call and Return
      1. 3.1.1 Call Instructions
        1. 3.1.1.1 Indirect Calls
        2. 3.1.1.2 Direct Calls
      2. 3.1.2 Return Instruction
      3. 3.1.3 Pipeline Conventions
      4. 3.1.4 Weak Functions
    2. 3.2 Register Conventions
      1. 3.2.1 Argument Registers
      2. 3.2.2 Callee-Saved Registers
    3. 3.3 Argument Passing
      1. 3.3.1 Passing 16-Bit Arguments
      2. 3.3.2 Passing Longer Arguments
      3. 3.3.3 C++ Argument Passing
      4. 3.3.4 Passing Structs and Unions
      5. 3.3.5 Stack Layout of Arguments Not Passed in Registers
      6. 3.3.6 Frame Pointer
    4. 3.4 Return Values
    5. 3.5 Structures and Unions Passed and Returned by Reference
    6. 3.6 Conventions for Compiler Helper Functions
    7. 3.7 Prolog and Epilog Helper Functions
    8. 3.8 Scratch Registers for Functions Already Seen
    9. 3.9 Interrupt Functions
  5. 4 Data Allocation and Addressing
    1. 4.1 Data Sections and Segments
    2. 4.2 Data Blocking
    3. 4.3 Addressing Modes
    4. 4.4 Allocation and Addressing of Static Data
      1. 4.4.1 Addressing Methods for Static Data
      2. 4.4.2 Placement Conventions for Static Data
        1. 4.4.2.1 Abstract Conventions for Addressing
      3. 4.4.3 Initialization of Static Data
    5. 4.5 Automatic Variables
    6. 4.6 Frame Layout
      1. 4.6.1 Stack Alignment
      2. 4.6.2 Register Save Order
    7. 4.7 Heap-Allocated Objects
  6. 5 Code Allocation and Addressing
    1. 5.1 Computing the Address of a Code Label
    2. 5.2 Calls
      1. 5.2.1 Direct Call
      2. 5.2.2 Far Call Trampoline
      3. 5.2.3 Indirect Calls
  7. 6 Helper Function API
    1. 6.1 Floating-Point Behavior
    2. 6.2 C Helper Function API
    3. 6.3 Floating-Point Helper Functions for C99
  8. 7 Standard C Library API
    1. 7.1  About Standard C Libraries
    2. 7.2  Reserved Symbols
    3. 7.3  <assert.h> Implementation
    4. 7.4  <complex.h> Implementation
    5. 7.5  <ctype.h> Implementation
    6. 7.6  <errno.h> Implementation
    7. 7.7  <float.h> Implementation
    8. 7.8  <inttypes.h> Implementation
    9. 7.9  <iso646.h> Implementation
    10. 7.10 <limits.h> Implementation
    11. 7.11 <locale.h> Implementation
    12. 7.12 <math.h> Implementation
    13. 7.13 <setjmp.h> Implementation
    14. 7.14 <signal.h> Implementation
    15. 7.15 <stdarg.h> Implementation
    16. 7.16 <stdbool.h> Implementation
    17. 7.17 <stddef.h> Implementation
    18. 7.18 <stdint.h> Implementation
    19. 7.19 <stdio.h> Implementation
    20. 7.20 <stdlib.h> Implementation
    21. 7.21 <string.h> Implementation
    22. 7.22 <tgmath.h> Implementation
    23. 7.23 <time.h> Implementation
    24. 7.24 <wchar.h> Implementation
    25. 7.25 <wctype.h> Implementation
  9. 8 C++ ABI
    1. 8.1  Limits (GC++ABI 1.2)
    2. 8.2  Export Template (GC++ABI 1.4.2)
    3. 8.3  Data Layout (GC++ABI Chapter 2)
    4. 8.4  Initialization Guard Variables (GC++ABI 2.8)
    5. 8.5  Constructor Return Value (GC++ABI 3.1.5)
    6. 8.6  One-Time Construction API (GC++ABI 3.3.2)
    7. 8.7  Controlling Object Construction Order (GC++ ABI 3.3.4)
    8. 8.8  Demangler API (GC++ABI 3.4)
    9. 8.9  Static Data (GC++ ABI 5.2.2)
    10. 8.10 Virtual Tables and the Key function (GC++ABI 5.2.3)
    11. 8.11 Unwind Table Location (GC++ABI 5.3)
  10. 9 Exception Handling
    1. 9.1  Overview
    2. 9.2  PREL31 Encoding
    3. 9.3  The Exception Index Table (EXIDX)
      1. 9.3.1 Pointer to Out-of-Line EXTAB Entry
      2. 9.3.2 EXIDX_CANTUNWIND
      3. 9.3.3 Inlined EXTAB Entry
    4. 9.4  The Exception Handling Instruction Table (EXTAB)
      1. 9.4.1 EXTAB Generic Model
      2. 9.4.2 EXTAB Compact Model
      3. 9.4.3 Personality Routines
    5. 9.5  Unwinding Instructions
      1. 9.5.1 Common Sequence
      2. 9.5.2 Byte-Encoded Unwinding Instructions
    6. 9.6  Descriptors
      1. 9.6.1 Encoding of Type Identifiers
      2. 9.6.2 Scope
      3. 9.6.3 Cleanup Descriptor
      4. 9.6.4 Catch Descriptor
      5. 9.6.5 Function Exception Specification (FESPEC) Descriptor
    7. 9.7  Special Sections
    8. 9.8  Interaction With Non-C++ Code
      1. 9.8.1 Automatic EXIDX Entry Generation
      2. 9.8.2 Hand-Coded Assembly Functions
    9. 9.9  Interaction With System Features
      1. 9.9.1 Shared Libraries
      2. 9.9.2 Overlays
      3. 9.9.3 Interrupts
    10. 9.10 Assembly Language Operators in the TI Toolchain
  11. 10DWARF
    1. 10.1 DWARF Register Names
    2. 10.2 Call Frame Information
    3. 10.3 Vendor Names
    4. 10.4 Vendor Extensions
  12. 11ELF Object Files (Processor Supplement)
    1. 11.1 Registered Vendor Names
    2. 11.2 ELF Header
    3. 11.3 Sections
      1. 11.3.1 Section Indexes
      2. 11.3.2 Section Types
      3. 11.3.3 Extended Section Header Attributes
      4. 11.3.4 Subsections
      5. 11.3.5 Special Sections
      6. 11.3.6 Section Alignment
    4. 11.4 Symbol Table
      1. 11.4.1 Symbol Types
      2. 11.4.2 Common Block Symbols
      3. 11.4.3 Symbol Names
      4. 11.4.4 Reserved Symbol Names
      5. 11.4.5 Mapping Symbols
    5. 11.5 Relocation
      1. 11.5.1 Relocation Types
        1. 11.5.1.1 Absolute Relocations
        2. 11.5.1.2 PC-Relative Relocations
        3. 11.5.1.3 Relocations in Data Sections
        4. 11.5.1.4 Relocations for C28x Instructions
        5. 11.5.1.5 Other Relocation Types
      2. 11.5.2 Relocation Operations
      3. 11.5.3 Relocation of Unresolved Weak References
  13. 12ELF Program Loading and Linking (Processor Supplement)
    1. 12.1 Program Header
      1. 12.1.1 Base Address
      2. 12.1.2 Segment Contents
      3. 12.1.3 Thread-Local Storage
    2. 12.2 Program Loading
  14. 13Build Attributes
    1. 13.1 About Build Attributes
    2. 13.2 C28x ABI Build Attribute Subsection
    3. 13.3 Build Attribute Tags
  15. 14Copy Tables and Variable Initialization
    1. 14.1 About Copy Tables
    2. 14.2 Copy Table Format
    3. 14.3 Compressed Data Formats
      1. 14.3.1 RLE
      2. 14.3.2 LZSS Format
    4. 14.4 Variable Initialization
  16. 15Revision History
    1.     188

Volatile Bit Fields

A volatile bit field is one declared with the C volatile keyword. When a volatile bit field is read, its container must be read exactly once using the appropriate access for the entire container.

When a volatile bit field with a size less than its container is written, its container must be read exactly once and written exactly once using the appropriate access. The read and the write are not required to be atomic with respect to each other.

The compiler does not use a narrower type for volatile bit-fields; it will instead use exactly the declared type.

When a volatile bit-field with a size exactly equal to the container size is written, it is unspecified whether the read takes place. Because such reads are unspecified, it is not safe to interlink object files compiled with different implementations if they both write to a volatile bit-field with exactly the width of its container. For this reason, using volatile bit-fields in external interfaces should be avoided.

Multiple accesses to the same volatile bit field, or to additional volatile bit fields within the same container may not be merged. For example, an increment of a volatile bit field must always be implemented as two reads and a write. These rules apply even when the width and alignment of the bit field would allow more efficient access using a narrower type. For a write operation the read must occur even if the entire contents of the container will be replaced. If the containers of two volatile bit fields overlap then access to one bit field will cause an access to the other.

An access to 'a' will also cause an access to 'b', but not vice-versa. If the container of a non-volatile bit field overlaps a volatile bit field then it is undefined whether access to the non-volatile field will cause the volatile field to be accessed.